README.TXT for INSITE CENSE Version 4.0.4

CONTENTS

    INSITE CENSE Overview
    Cummins Y2000 Readiness Disclosure
    Enhancements
    Features
    Uninstall
    Known Issues
    Service and Support

---------------------
INSITE CENSE Overview
---------------------

INSITE CENSE Version 4.0.4 is the fourth INSITE CENSE release
for the K38/K50 and QSK19 engine series and the second INSITE
CENSE release for the new QST30 industrial engine series. 
This version does not require INSITE base but will use ESDN 
to download a calibration to a module. As with all INSITE 
releases this release uses the standard software security 
scheme.

INSITE CENSE will install like all other Windows products. A
separate program manager group window will be created called
INSITE CENSE. INSITE CENSE will have its own icon. A
separate icon will be created for the CENSE fault
information system and the readme help.

----------------------------------
Cummins Y2000 Readiness Disclosure
----------------------------------

Cummins has a good faith belief that this Personal Computer (PC) 
based software product is Year 2000 compliant, as defined by 
Cummins in our Compliance Statement. However, For this Cummins 
(PC) based software product to operate correctly in the year 2000, 
the PC on which the product is installed must also be Year 2000 
compliant.  Being Year 2000 compliant includes, but is not limited 
to, ensuring that the operating system (e.g. Windows 95), the 
computer BIOS, and the PC hardware are also Year 2000 compliant.  
If any of these PC "components" are not Year 2000 compliant, 
Cummins cannot provide any assurances that the PC software will 
operate as designed. Please see the Cummins Year 2000 Compliance 
Statement for more information.

------------
Enhancements
------------

The enhancements for INSITE CENSE Version 4.0.4 include the
following items:

    QSK45/60 Fault Information System. 	    

    RF Modem Support.  A RF Modem mode was added to the
    software to provide support for the Freewave short
    range RF modem system.  In this mode, data may be 
    retrieved, viewed and modified without having a direct
    hard wire connection to the CENSE ECM.

    Y2000 Support.  INSITE for CENSE has been modified to 
    incorporate the Y2K compliant version of security.

    CENSE V2.0.3 is no longer supported.
 
--------
Features
--------

INSITE for CENSE contains features specific to the new CENSE
engine monitoring system.  These features include:

    Job
        New
        Open
        Close
        Delete
        Summary Info
        Print
            Print Normal
            Print Narrow
        Print Setup
        Import/Export
            Import Jobs
            Export Jobs
            Export Data (To Inform)
        Exit

    Adjustments Menu
        Real-Time Clock
        Maintenance
        Trend Datalog
        Dataplate
        Dispatch 
        CENSE Data Reset
        Duty Cycle and Fuel Consumption

    View Menu
        Fault Data
        Engine Start Log
        Engine Hourmeters
        Maintenance
        System ID and CENSE Dataplate
        Dispatch
        Trend Data
        Duty Cycle and Fuel Consumption
        Fault Information System

    Monitor Menu
        Signal Cylinder Diagnostics Data
        Sensor Data
            Graphical Monitor
            Textual Monitor
            Data Logger
            Graphical Playback   

    Tools Menu
        Data Extraction
        Calibration
        INFORM

    System
        Preferences
        User Options
        Units of Measure


INSITE CENSE will work under Windows 3.1 and Windows 95
operating systems.

---------
Uninstall
---------

Version 4.0.4 of INSITE CENSE supports an uninstall
feature. This uninstall program is located in the INSITE
CENSE program group. The uninstall process will not remove
all of the files associated with INSITE CENSE. Any data
contained in the export, usrdata, and log directories will
not be removed. The database information located in the db
directory will only be removed if the user requests it
during the uninstall process. The Microsoft Windows OLE and
ODBC support which was installed, will not be automatically
removed. These components will not be automatically removed
because they may be shared with other applications currently
existing on your machine which were installed before or
after INSITE CENSE. The list of files which were not removed
include:

    OLE Files
    =========
        File Name           Location
        ---------           --------
        compobj.dll         windows\system
        ole2.dll            windows\system
        ole2.reg            windows\system
        ole2conv.dll        windows\system
        ole2disp.dll        windows\system
        ole2nls.dll         windows\system
        ole2prox.dll        windows\system
        stdole.tlb          windows\system
        storage.dll         windows\system
        typelib.dll         windows\system
        vshare.386          windows\system
        
    ODBC Files
    ==========
        File Name           Location
        ---------           --------
        ctl3dv2.dll         windows\system
        odbc.dll            windows\system
        odbcadm.txt         windows\system
        odbccurs.dll        windows\system
        odbcinst.dll        windows\system
        odbcinst.hlp        windows\system
        odbc.ini            windows\system
        odbcinst.ini        windows\system
        
    Database Files
    ==============
        File Name           Location
        ---------           --------
        dbl50w.dll          windows\system
        rtdsk50w.exe        windows\system
        wl50en.dll          windows\system
        wod50w.dll          windows\system

    Other Files
    ===========
        File Name           Location
        ---------           --------
        cense.ini           \windows
        azmemory.drv        \windows\system
        *.*                 \intelect\cense\log
        *.*                 \intelect\cense\export
        *.*                 \intelect\cense\usrdata
        *.*                 \intelect\cense\db 
                               (if database not 
                               removed on uninstall)

------------                
Known Issues
------------

A main feature of INSITE CENSE allows the user to store
trend data and fault log information to a job. INSITE CENSE
does not create a new job image every time data is accessed
from the module. If module data is reset, and the current
job is not closed before viewing the reset module data, the
information in the open job will be updated and the original
job information will be lost. To eliminate the possibility
of overwriting job data, the current job should be closed
after resetting module data. To view the reset module data,
a new job should then be opened.

General search in ESDN is not available for CENSE. The
general search button on the tool bar will take the user to
the calibration search dialog and then to the recalibrate
ECM dialog instead of the general search dialog.

INSITE CENSE can not move an ALL ECM server or client
key. When installing INSITE CENSE and the "Move security
onto hard drive" button is selected on the setup dialog an
error message will be generated. Clicking "OK" will take the
user back to the setup dialog without moving the security
key to the hard drive.

-------------------
Service and Support
-------------------

To receive support and service information for INSITE CENSE
Version 4.0.4, call these numbers:

    Phone:   812-377-8136
        
    Fax:     812-377-6340
 
Before you Call

Before you place a support call, you may be able to
troubleshoot the problem yourself by trying these steps:

    1. If necessary, exit from your network and restart the
       software locally.

    2. If the problem persists, turn your computer off, then
       on again, and re-start INSITE.

If the problem persists, gather the following information to
discuss with your Cummins support representative:

    - The exact wording of any error messages that display.

    - What you were doing when the problem occurred.

    - A printed report of the system produced by Microsoft's
      Diagnostic tools (MSD), which comes with Windows.